Station Runtime Pro (XL)
This XL example shows you a system architecture using an HMI and two web clients.
XL System architecture
This example architecture has the following components:
- Single HMI station with typical HMI functionality and twenty web clients
- Communicates with multipleRockwell Automation®controllers and multiple third-party controllers
- Acts as a client to multiple OPC UA servers
- Acts as an OPC UA server to one client
- Logs data to an internal database
- Exchanges data with external databases via ODBC
- Requires event logging, alarming, recipes, and basic PDF reporting
The following picture shows example runtime sizing for a package that includes these application components.
HMI with Extensibility

Provide Feedback