Station Runtime Lite (XS)

This XS example shows you a system architecture using an Embedded Edge Compute module.
XS System architecture
A diagram of sample XS system.
This example architecture has the following components:
  • No HMI displays
  • Communicates with a
    Rockwell Automation®
    controller
  • Acts as an OPC UA server
  • Logs data to an internal database
  • One web client
The following picture shows example runtime sizing for a package that includes these application components.
XS with Embedded Edge Compute module
An example runtime sizing for a package in a XS system.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal