Station Runtime Lite (S)

This S example shows you a system architecture using a panel PC and two controllers.
S System architecture
A diagram of sample S system.
This example architecture has the following components:
  • Single HMI station (panel PC) with typical HMI functionality
  • Communicates with a
    Rockwell Automation®
    controller and a third-party controller
  • Logs data to an internal database
  • Requires event logging, alarming, recipes, and basic PDF reporting
The following picture shows example runtime sizing for a package that includes these application components.
S with panel PC and multiple controllers
An example runtime sizing for a package in a S system.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal