Configure temperature controls

Create Label, Textbox, and Linear gauge objects to visualize and control the temperature variable.
  1. In
    Project view
    , double-click
    Page1 (type)
    .
    Page1 (type) opens in the editor.
  2. Right-click
    Page1 (type)
    and select
    New
    Base controls
    Label
    .
  3. In
    Properties
    , set
    Text
    to
    Temperature:
    .
  4. In
    Project view
    , right-click
    Page1 (type)
    and select
    New
    Base controls
    Text box
    .
  5. In
    Properties
    , create a dynamic link between
    Text
    and the
    Temperature
    variable.
    TIP: You can create the dynamic link by dropping the
    Temperature
    variable from
    Project view
    into the
    Text
    property value of the
    Text box
    in
    Properties
    .
  6. In
    Project view
    , right-click
    Page1 (type)
    and select
    New
    Base controls
    Linear gauge
    .
  7. In
    Properties
    , create a dynamic link between
    Value
    and the
    Temperature
    variable.
  8. In the editor, arrange the objects according to your preferences.
Temperature controls in the top-right corner
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal