Configure a widget to display logged alarms

Add a widget that displays historical data about alarms at runtime.
  1. From the toolbar, select
    Template Libraries
    .
  2. In , search for
    Alarm History Grid with filter
    .
  3. Under
    Components
    , drag
    Alarm History Grid with filter
    onto
    Page3 (type)
    in
    Project view
    .
  4. Select
    Close
    .
  5. In
    Project view
    , select
    FilteredAlarmHistoryGrid1
    .
  6. In
    Properties
    , set
    Horizontal alignment
    to
    Stretch
    .
    The object adjusts its width to the container at runtime.
  7. Create a dynamic link between
    AlarmsEventLogger
    and
    ProjectName
    Loggers
    AlarmsEventLogger1
    .
    For more information about dynamic links, see #.
Filtered Alarms History Grid with filter in Page3
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal