Purchase FactoryTalk Optix Runtime

To run FactoryTalk Optix Runtime, purchase an entitlement on the Commerce Portal and allocate that entitlement to your Organization. A FactoryTalk Optix Runtime license allows you to run FactoryTalk Optix Applications on physical or virtual HMI devices. Devices that are not activated operate in a 2-hour demo mode.
FactoryTalk Optix Runtime is only available with a perpetual license today. The FactoryTalk Optix Studio Emulator does not require a runtime license.
  1. Navigate to the Commerce Portal page and log in with your MyRockwell account.
  2. Paste the catalog number from the Runtime Sizing tool in Search at the top of the Commerce Portal page.
  3. Paste the catalog and click the cart icon to add the catalog number to your cart.
  4. (optional) If required, change the quantity to purchase.
    TIP: If you did not copy the FactoryTalk Optix Runtime catalog number when determining the FactoryTalk Optix Runtime package, select the catalog number from the list, scroll to FactoryTalk Optix, select
    CONTINUE
    , select your package, customize, select quantity and then select Add to cart.
  5. Once FactoryTalk Optix Runtime is added to your cart, select CHECKOUT.
  6. Review pricing with your Distributor, review your cart, and select CHECKOUT.
  7. Go to
    My Subscriptions/Manage Licenses
    to confirm your order status. You can also select
    Manage Licenses
    from the order confirmation page.
  8. Confirm your Shipping, Billing, Contract Details and Order Summary and submit the order.
  9. Once the status is
    Active
    , your entitlement is available in FactoryTalk Hub.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal