Runtime sizing tool

The runtime sizing tool lets you enter the details of your project and recommends the feature token package that you need. The available packages include two options of each Station Runtime-Lite, Station Runtime-Standard, and Station Runtime-Pro.
To determine the runtime package that you need for your application, use the Runtime Sizing tool within the
FactoryTalk® Optix
page.
  1. Select
    FactoryTalk® Optix
    from the list of available applications.
    This image shows the available applications in FactoryTalk Optic
  2. Select Runtime Sizing from the top navigation bar.
    This image shows the Runtime Sizing tab in FactoryTalk Optix.
  3. Follow the wizard to select the features your application needs.
For example, if you select these features:
Example sizing selections
Wizard Category
Example Selection
Select presentation
Web HMI Client
Select features
  • Data Logger
  • Database
Controller connections
Rockwell EtherNet/IP
  • Single connection
  • Rockwell Hardware
Select interoperability
  • OPC UA Client None
  • OPC UA Server 1 token
You see these recommended runtime packages:
Example recommended runtime packages
This image shows recommended runtime packages in FactoryTalk Optix.
Select the package you want to see the associated catalog number for purchase via the Commerce Portal.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal