Deployment guidelines

After you create your project, you need to deploy it to a target device. This section helps you to ensure that you deploy it correctly.
  1. Confirm that the
    FactoryTalk® Optix
    Application Update Service runs on the target device.
    The Application Update Service is part of the Runtime Tools.
    OptixPanel
    and Embedded Edge Compute devices come with Runtime Tools pre-installed.  You must install Runtime tools on other target devices.
    To operate correctly, the Application Update Service requires the TCP port 49100 to be reachable and a valid username with a configured password.
  2. If needed, assign entitlements to target devices.
    Some target devices come with pre-assigned entitlements. You only need to assign an entitlement if you upgrade a pre-assigned entitlement or if the target device has no entitlement.
  3. Configure the target device to accept the application.
  4. Deploy the application to the target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal