Application Code Libraries/Trusted Content

Rockwell Automation®
has built libraries of standard application content to help you easily integrate automation products into systems. This application content helps engineers create automation projects from standardized, lifecycle-managed, application-focused libraries in an efficient way.
Reduce design cost, build projects faster, and drive consistent results with the
Rockwell Automation®
Library of Process Objects (
PlantPAx®
Libraries), Device Object Libraries, and Machine Builder Libraries.
The following libraries and version of
FactoryTalk® Optix
are compatible:
Compatible Libraries
Library
FactoryTalk® Optix
1.5 Compatible Version
FactoryTalk® Optix
1.4 Compatible Version
Power Device
3.06
3.05
Safety Device
1.06
1.05
Network Device
12.05
12.04
Condition Monitoring Device
1.03
1.02
Hardy Device
1.01
1.00
IO Device
5.05
IO-Link Device
3.03
Mettler Toledo Device
1.01
Plex APM
1.01
1.00
Plex QMS
1.01
1.00
Fiix®
1.01
1.00
You can download the libraries at the Product Compatibility and Download Center (PCDC). The PCDC is available at rok.auto/pcdc.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal