FactoryTalk Optix Studio web editor

You can use
FactoryTalk Optix Studio
in a web browser through
FactoryTalk Hub
.

Editor features support

FactoryTalk Optix Studio web editor
supports all
FactoryTalk Optix Studio desktop editor
features except for:
  • Save logs from the
    Output
    tabs.
  • Edit NetLogic files.
  • Display paths in logs in the
    Output
    tabs.
  • Add files and images by dragging and dropping them into
    FactoryTalk Optix Studio web editor
    .
  • Restart the application at runtime by using the
    Commands
    Core commands
    Restart
    method.

Emulator features support

FactoryTalk Optix Studio web editor
emulator supports all features of
FactoryTalk Optix Studio desktop editor
emulator except for:
  • Control the
    WebBrowser
    object in the runtime emulator.
  • Control the
    PDFViewer
    object in the runtime emulator.
  • Control the
    Video
    object in the runtime emulator.
  • Control the
    Window
    object in the runtime emulator.
  • Cursor does not indicate areas in which you cannot drop elements.

Change to the ImagePosition property for a button

The data type for the
ImagePosition
property changed to
ButtonImagePosition
. Any existing NetLogic scripts that assign a value to
Position
need to be changed to
ImagePosition
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal