Corrected anomalies in this release
The list identifies the anomalies corrected in
FactoryTalk Optix
1.6.x.Custom library elements do not appear without restarting FactoryTalk Optix
[2371413]
Elements added to a custom library do not appear in
Libraries
search
until you restart FactoryTalk Optix. This anomaly corrected in version 1.6.0
This anomaly first identified in version 1.3.0.
Spinbox may display value in accurately [3685185]
Using a datatype other than the default on a UI control may result in a loss of precision
in the value displayed.
This anomaly corrected in version 1.6.0
This anomaly first identified in version 1.5.0.
Incorrect status under Micro Controller Driver [3774138]
When multiple stations are used, non-active screens with data from stations that do not
have data on active screen, may not show correct status. See application notes for
additional information.
This anomaly corrected in version 1.6.0.
This anomaly first identified in version 1.5.0.
PlantPAx process instruction HMI extended tag properties are not imported with L5X
offline tag import [3890998]
Importing tags using an L5X file does not import the PlantPAx process instruction HMI
extended tag properties. Import the properties offline using a Logix v37 ACD file or online
from the controller.
This anomaly corrected in version 1.6.0.
This anomaly first identified in version 1.5.0.
PDF reports are not generated initially when using the Emulator [3880034]
When using the emulator, PDF report files are not generated on initial button press. Press
the button again to generate the report.
This anomaly corrected in version 1.6.0.
This anomaly first identified in version 1.5.0.
The FactoryTalk Optix web editor may become unresponsive during tag import operations
[3795569]
The
FactoryTalk Optix
web editor may become unresponsive
during large offline tag import operations. Try importing the tags online from the
controller or use the FactoryTalk Optix
desktop editor.This anomaly corrected in version 1.6.0.
This anomaly first identified in version 1.5.0.
Provide Feedback