Rehost a FactoryTalk Optix Studio Pro entitlement

You can rehost the
FactoryTalk® Optix Studio
Pro entitlement by using either the
FactoryTalk® Optix Studio
desktop application or the
FactoryTalk® Optix
landing page.
Follow one of the following procedures to reallocate a
FactoryTalk® Optix Studio
Pro entitlement from a user to another.

Rehosting from the desktop application

  1. Make sure that your device is connected to the Internet.
  2. Access the
    FactoryTalk® Optix Studio
    desktop application.
  3. Click the
    Login
    icon at the top right corner.
  4. On the drop-down menu, select
    Rehost entitlement
    .

Rehosting from the
FactoryTalk® Optix
landing page

  1. Make sure that your device is connected to the Internet.
  2. Access the
    FactoryTalk® Optix
    landing page.
  3. Select
    Entitlements
    Organization entitlements
    .
  4. Click the
    Rehost
    button located in the rightmost column next to the
    FactoryTalk® Optix Studio
    Pro entitlement that you want to rehost.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal