Install Runtime Tools on Windows devices
Once you download the
FactoryTalk® Optix™
Runtime Tools installation package, install the Runtime Tools.
IMPORTANT:
If the Runtime device is not connected to the Internet, you cannot
download the installation package from the
FactoryTalk® Optix™
landing
page. Download the installation package to an online device and then transfer it to the
Runtime device by means of a USB drive.- When the download is complete, selectOpento open the download folder.
- In the download folder, double-click onFactoryTalk® Optix™Runtime Tools .exe file and wait for the installation process to complete.TheFactoryTalk® Optix™Application Update Service andFactoryTalk® Optix™Entitlement Manager are now installed.
TIP:
If the project includes an ODBC Database linked to a MySQL server, install a
MySQL ODBC connector
additional package that you can download from
the Microsoft products page.
TIP:
If the project includes an ODBC Database linked to an SQL server, install a
ODBC Driver 17 for SQL Server
additional package that you can
download from the Microsoft products page.
TIP:
To install
FactoryTalk® Optix™
Studio or the Windows Runtime
Tools or both in silent mode, run the following scripts in the Windows Command Prompt
terminal by replacing the <version>
placeholder accordingly.FTOptixStudioSetup_Win32_<version>.exe /Q
/IAcceptAllLicenseTerms
FactoryTalkOptixRuntimeToolsSetup_Win32_<version>.exe /Q
/IAcceptAllLicenseTerms
Silent mode is useful if you do not want to interact with the script and for various
automations.
Provide Feedback