Device Sizing

The
Device Sizing
calculator identifies the optimal device to run your
FactoryTalk® Optix
application efficiently.
To access the
Device Sizing
section of the
FactoryTalk® Optix
landing page:
  1. Select the
    Device Sizing
    tab.
  1. Review the
    Introduction
    section and then select
    Next
    .
  2. Complete:
    • Select items
      : Enter the quantity for each listed item that you want to use in your
      FactoryTalk® Optix
      application and then select
      Next
      .
      TIP:
      To expand a list item, click the arrow located next to the items.
      To view the item description, hover over an item.
    • Number of screens
      : Select the number of screens with the desired screen density for your project and then select
      Next
      .
      TIP: Click on the screen density images to enlarge them.
    • Recommended device
      : View a summary of your selections and the recommended device for your
      FactoryTalk® Optix
      application.
      TIP: The Device sizing tool estimates the necessary device memory space and the startup time required for the application
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal