Develop an animated side menu

Use value change animation to smoothly show and hide a side menu.
NOTE:
Download a sample project:
AnimateSideMenu.zip.
Side menu example
Prerequisites
  1. To develop the project
  2. Arrange the interface elements.
  3. Save the project.
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal