Develop an interface for switching locales
Create a localized label and two buttons that change the interface language.
Application example - English locale

Application example - Polish locale

NOTE:
Download a sample project:
SwitchLocales.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

Select
to run the project using the client
emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback