Publish the object

Add an OPC UA server and publish the object that exposes an OPC UA method.
  1. In
    Project view
    , right-click
    OPC-UA
    and select
    New
    OPC UA server
    .
    OPCUAServer
    appears under
    OPC-UA
    .
  2. In
    Properties
    , next to
    Nodes to publish
    , select
    Add
    .
    A configuration of nodes to be published appears under
    Nodes to publish
    .
  3. Under
    Configuration1
    , next to
    Nodes
    , select
    Add
    .
  4. From
    Project view
    , drag
    MyObject1
    next to
    Node1
    in
    Properties
    .
  5. (optional) Adjust other OPC UA server preferences. See Add an OPC UA server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal