ZipUnzip NetLogic

The Zip Unzip NetLogic enables you to create, extract, and password-protect ZIP archives.
IMPORTANT: This NetLogic uses a third-party library. For more information, see NuGet Gallery | SharpZipLib.

CreateZipArchive
method

Compress a file or a folder into a ZIP archive.
Takes the following properties:
Source
A full path to the file or folder to be compressed.
Target
A full path to the archive to generate.
Password
(Optional) The phrase that password-protects the generated archive.

UnzipArchive
method

Decompresses a ZIP archive.
Takes the following properties:
Source
A full path to the ZIP archive to decompress.
Target
A folder path where the archive contents will be extracted.
Password
(Optional) The phrase that may be needed to extract the archive.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal