Develop a contact form

Develop a contact form that sends emails to a predefined address.
Application example
TIP:
You can download a sample project from:
ContactForm.zip
Prerequisites
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal