Create a variable

Create a variable that indicates the current temperature.
  1. Create the variable:
    1. In
      Project view
      , right-click
      Model
      and select
      New
      Variable
      .
    2. Hover-over the variable, select
      Edit
      , and enter
      Temperature
      .
  2. Configure the variable:
    1. In
      Properties
      , select
      Int32
      and select
      Float
      .
    2. Right-click
      Temperature
      and select
      New
      Range
      .
    3. Under
      EURange
      , set
      High limit
      to
      100
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal