Create a linear gauge

Create a gauge that enables you to see and control the current temperature.
  1. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    Base controls
    Linear gauge
    .
  2. Configure the gauge:
    1. In
      Property
      , create a dynamic link between
      Value
      and
      ProjectName
      Model
      Temperature
      .
    2. Next to
      Warning zones
      , select
      Add
      .
    3. Under
      WarningZone1
      , create a dynamic link between
      From
      and
      ProjectName
      Alarms
      ExclusiveLevelAlarm1
      High limit
      For more information about dynamic links, see Create dynamic links.
    4. Under
      WarningZone1
      , create a dynamic link between
      To
      and
      ProjectName
      UI
      MainWindow (type)
      inearGauge1
      Maximum value
      .
      For more information about dynamic links, see Create dynamic links.
    5. Under
      WarningZone1
      , set
      Color
      to
      #fe1414
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal