Display a dialog on value change

Display a dialog box when variable value or tag value changes to a different value.
Application example
The panel displays when the spin box value changes.
NOTE:
Download a sample project:
DisplayDialog.zip
Prerequisites
  1. To develop the project
  2. Arrange the interface elements.
  3. Save the project.
Application design example
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal