Create an analog variable

Create an analog variable that indicates temperature.
  1. In
    Project view
    , right-click
    Model
    and select
    New
    Analog variable
  2. Configure the variable:
    1. In
      Properties
      , set the
      AnalogVariable1 (Float)
      property value to
      50
      .
    2. Next to the property value, select
      <None>
      and select
      Temperature: degree Fahrenheit
    3. Under
      EURange
      , set
      Low limit
      to
      -10
      .
    4. Set the
      High limit
      to
      60
      .
    5. Set the
      Constrain
      to
      True
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal