Develop a temperature change alarm
Develop an alarm that signals when temperature exceeds a set value.
Application example

NOTE:
Download a sample project:
TemperatureChangeAlarm.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

Select
to run the project using the client
emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback