Configure a recipes editor

Configure the recipes editor to manage recipes at runtime.
  1. From the toolbar, select
    Template Libraries
    .
  2. In , search for
    Recipes Editor
    .
  3. Under
    Components
    , drag
    Recipes Editor
    onto
    Page4 (type)
    in
    Project view
    .
  4. Select
    Close
    .
  5. In
    Project view
    , select
    RecipesEditor1
    .
  6. In
    Properties
    , set
    Horizontal alignment
    to
    Stretch
    .
    The object adjusts its width to the container at runtime.
  7. In
    Project view
    , select
    RecipesEditor1
    .
  8. In
    Properties
    , create a dynamic link between
    RecipeSchema
    and
    ProjectName
    Recipes
    RecipeSchema1
    .
    For more information about dynamic links, see Create dynamic links.
  9. Right-click
    RecipesEditor1
    and select
    Execute Setup
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal