Configure a navigation panel

Configure a navigation panel to switch between different panels at runtime.
  1. In
    Project view
    , double-click
    MainWindow (type)
    .
    The window type opens in the editor.
  2. Right-click
    MainWindow (type)
    and select
    New
    Containers
    Navigation panel
    .
    Navigation panel appears in the main window and is not positioned.
  3. In
    Properties
    , set
    Horizontal alignment
    and
    Vertical alignment
    to
    Stretch
    .
    The navigation panel occupies the entire height and width of the main window and covers the logo.
  4. Set
    Top margin
    to
    55
    .
    The navigation panel no longer covers the logo.
  5. Drag
    Page1 (type)
    ,
    Page2 (type)
    ,
    Page3 (type)
    , and
    Page4 (type)
    onto
    NavigationPanel1
    .
Navigation pane with empty pages
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal