Associate the LED status with the switch

Turn the LED object on and off with the switch.
  1. In
    Project view
    , select
    LED1
    .
  2. In
    Properties
    , create a dynamic link between
    Active
    and
    ProjectName
    UI
    Pages
    Page1 (type)
    Switch1
    Checked
    .
    For more information about dynamic links, see Create dynamic links.
LED toggle
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal