Configure a switch to simulate alarms

Configure a switch that simulates Motor1 alarms.
  1. In
    Project view
    , double-click
    Page2 (type)
    .
  2. Right-click
    Page2 (type)
    and select
    New
    Base controls
    Switch
    .
  3. In
    Properties
    , create a dynamic link between
    Checked
    and the
    Motor1Alarm
    variable.
    For more information about dynamic links, see Create dynamic links.
  4. In the editor, arrange
    Switch1
    according to your preferences.
Switch to simulate alarms at the bottom of Page2
At runtime, toggle the switch to trigger an alarm.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal