FactoryTalk Optix Studio

FactoryTalk Optix Studio
is an integrated development environment with a framework of functional modules for designing and compiling HMI or Internet of Things (IoT) applications.
FactoryTalk Optix Studio
includes a library of predefined objects that support the modular design of graphical interfaces, features, and logic operations of an HMI application. By using specific C# language scripts, you can automate various actions in the design phase and add customized functions to projects.

Desktop and web editors

FactoryTalk Optix Studio
is available as a web and a desktop development environment that you use to build
FactoryTalk Optix Applications
  and deploy them to client systems. You access
FactoryTalk Optix Studio web editor
through
FactoryTalk Hub
.
If there is an Internet connection outage:
  • FactoryTalk Optix Studio web editor
    tries to reconnect to the Internet every 5 seconds. During that period, you cannot interact with
    FactoryTalk Optix Studio web editor
    . Once
    FactoryTalk Optix Studio web editor
    reconnects to the Internet, you can continue where you left off.
  • FactoryTalk Optix Application
    displays the message "
    Server unreachable
    " after 10 seconds. When the
    FactoryTalk Optix Application
    reconnects to the Internet, the application attempts to restore the user session and the interface displays.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal