Debug NetLogic remotely with Visual Studio

With
Visual Studio®
, you can remotely debug a runtime NetLogic on Windows systems.
TIP: Remote debugging is not possible on HMIs for security reasons. For more information about remote debugging, see Remote debugging - Visual Studio (Windows) | Microsoft Learn.
Prerequisites
  • On the development machine, download
    Visual Studio
    and set as the default code editor. See Set the default code editor.
  • Verify that the target machine and the development machine are connected to the same network.
  1. To debug runtime NetLogic remotely
  2. Configure the remote Windows machine as a target in
    FactoryTalk Optix Studio
    . See Add a target device.
  3. Stop the debugging process, edit the code, and repeat the procedure.
    TIP: To stop the remote debugging process, close the Remote Debugger desktop application or stop debugging in
    Visual Studio
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal