IUAObject.UAEvent

This event occurs when the project object to which the
IUAObject
C# object refers generates any OPC UA event.
event EventHandler<UAEventArgs> UAEvent;

Event handler

public delegate void UAEvent(object sender, UAEventArgs e);

Event handler arguments

sender
(object)
A C# object that corresponds to the object of the project origin of the event.
e
(UAEventArgs)
A C# object that contains the following properties:
EventType
(IUAObjectType)
The node of the type of event generated.
Arguments
(UAEventArgumentList)
A C# object that contains the arguments of the generated event.

Example

The
Button1_UAEvent
method runs each time the
Button1
project button generates any event (for example,
OnMouseClick
,
OnMouseDown
, or
OnMouseUp
).
public override void Start() { var button1 = Owner.Get<Button>("Button1"); button1.UAEvent += Button1_UAEvent; } private void Button1_UAEvent(object sender, UAEventArgs e) { var label1 = Owner.Get<Label>("Label1"); var button1 = (Button)sender; label1.Text = "Event on " + button1.BrowseName + " of type " + e.EventType.BrowseName + " , "; }
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal