Add Edge App Broker to your project
Ensure that the following items are installed on your system:
- Edge App Broker
- Edge applications
TIP:
To obtain the Edge App Broker and Edge
applications, contact your Rockwell Automation representative.
- In your project, right-click the top node, and select.
- Right-clickEdgeApplicationsfolder, and selectEdge App Broker.
- InProperties, configure the Edge App Broker addon.Available Edge App Broker applications depend on what is installed on your system.
- Select models that you want to be available for the broker:
- InProperties, select.
- (optional) Rename the model.
- Next to the model, select.Add Dynamic Link
- From the menu, select the folder you want to use.Rockwell Automation recommends using the contents of theModelfolder for models.
Provide Feedback