LogicObject
Variable: direct access to the NetLogic object

Each NetLogic displays a
LogicObject
variable, which represents the same NetLogic node. It is useful for directly accessing the node.

Examples

This example shows the value of the
Speed
variable contained in the NetLogic set to
100
LogicObject.GetVariable("Speed").Value = 100;
This example shows the value of the
Speed
variable assigned to the
speed
C# integer variable.
int speed = LogicObject.GetVariable("Speed").Value;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal