IUAVariable.RemoteWrite(value, timeoutMilliseconds)

Writes the value passed in the first argument in the variable on which it invokes. The second optional argument sets the timeout period.
void RemoteWrite(UAValue
value
, double
timeoutMilliseconds
);

Arguments

value
(UAValue)
The value to write.
timeoutMilliseconds
(double)
The timeout period, expressed in milliseconds, after which the API throws an exception.
TIP: If not specified, the default value of the argument is
30000
(30 seconds).

Example

In the following example, the
42
value is written in the
Speed
variable.
var currentSpeed = Project.Current.GetVariable("Model/Motor/Speed"); currentSpeed.RemoteWrite(42);
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal