InformationModel.RemoteWrite(variableValues, timeoutMilliseconds)

Writes the values in the variables on interest. The second optional argument sets the timeout period.
static void RemoteWrite(IEnumerable<RemoteVariableValue> variableValues, double timeoutMilliseconds);

Arguments

variableValues
(IEnumerable<RemoteVariable>)
The list of the variable values that you want to write, expressed as a pair of the
RemoteVariableValue
class following properties:
Variable
(IUAVariable)
The variable.
Value
(UAValue)
The value of the variable.
timeoutMilliseconds
(double)
The timeout period, expressed in milliseconds, after which the API throws an exception.
TIP: If not specified, the default value of the argument is
30000
(30 seconds).

Example

In the following example, the values of two tag variables are written: the
0
value for the
tag3
variable, and the
123
value for the
tag1
variable. The variables of interest are included and searched with the
Get()
method in the
remoteVariableValues
list, which is passed as argument of the
RemoteWrite()
method.
var tag1 = Project.Current.Get<Tag>("CommDrivers/CodesysDriver1/CodesysStation1/Tags/Application/PLC_PRG/VAR1"); var tag3 = Project.Current.Get<Tag>("CommDrivers/CodesysDriver1/CodesysStation1/Tags/Application/PLC_PRG/VAR3"); var remoteVariableValues = new List<RemoteVariableValue>() { new RemoteVariableValue(tag3, 0), new RemoteVariableValue(tag1, 123) }; InformationModel.RemoteWrite(remoteVariableValues);
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal