Manage templates
Use C# APIs to import templates from template libraries and resolve conflicts by
running a design time NetLogic.
TIP:
You can only import templates through C# APIs with
the
Show feature preview
option enabled. For more information,
see Set options.Consider the following while using C# APIs to manage templates:
- Before importing templates, commit the project to create a snapshot of the current project state. See Commit changes. Committing the project enables you to roll back to the previous project state at any time. See Restore a project to a commit.
- You can only import templates compatible with yourFactoryTalk Optix Studioversion. You cannot update templates incompatible with yourFactoryTalk Optix Studioversion through C# APIs.
- You can only import templates under compatible parent nodes.
- You can only import local templates.
- When you import a template of a UI object, you may need to reposition or instantiate the object.
Provide Feedback