InformationModel.AddTranslation(localizedText, localizationDictionary)

Adds a new key in the project
LocalizationDictionary
, which name corresponds to the value of the
TextId
property of the first argument.
If the first argument also contains the
LocaleId
and
Text
properties, it also adds the translated string. The second argument is optional and indicates the
LocalizationDictionary
to which the key is added.
IMPORTANT: You must specify the second argument if the project contains more than one
LocalizationDictionary
.
void AddTranslation(LocalizedText
localizedText
, IUAVariable
localizationDictionary
);

Arguments

localizedText
(LocalizedText)
A C# object with properties that identify the key and any translated string to add.
localizationDictionary
(IUAVariable)
A C# object that represents a
LocalizationDictionary
.

Example

The following example shows an API that adds a
NewKey
key and a
New translation
string for the
en-US
locale.
var myLocalizedText = new LocalizedText("NewKey", "New translation", "en-US"); InformationModel.AddTranslation(myLocalizedText);
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal