ResourceURI.FromURI(uri)

Returns a C# object of the
ResourceURI
type, with the
URIType
type pf
URI
and that contains an absolute path to a generic resource.

Arguments

uri
(string)
An absolute path of a generic resource, usually a network path or a website address.

Returns

ResourceURI
A C# object that contains the path indicated in the argument.

Example

Below is an example in which the API returns a C # website object of the
ResourceURI
type that contains the
https://www.rockwellautomation.com/
URL.
var website = ResourceURI.FromURI("https://www.rockwellautomation.com/");
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal