RemoteVariableSynchronizer.Remove(variables)

Depending on the overload, removes a variable or a list of variables from the
RemoteVariableSynchronizer
object on which it is invoked.
void public void Remove(IUAVariable variables); void public void Remove(RemoteVariable variables); void public void Remove(IEnumerable<IUAVariable> variables); void public void Remove(IEnumerable<RemoteVariable> variables);

Argument

variables
(IUAVariable)
The
IUAVariable
C# object to add to the object on which the method is invoked.
variables
(RemoteVariable)
The
RemoteVariable
C# object that identifies a cell of a one-dimensional or multidimensional array to be added to the object on which the method is invoked.
variables
(IEnumerable<IUAVariable>)
The
IUAVariable
list to be added to the object on which the method is invoked.
variables
(IEnumerable<RemoteVariable>)
The
RemoteVariable
list to be added to the object on which the method is invoked.

Examples

In the following example, a variable
speed
is removed from the
variableSynchronizer
object.
variableSynchronizer.Remove(speed);
In the following example, the
10
index variable is removed from the
variableSynchronizer
object within the
arrayVariable
array.
variableSynchronizer.Remove(new RemoteVariable(arrayVariable, 10));
In the following example, the
10.5
index variable is removed from the
variableSynchronizer
object within the
scalarVariable
multidimensional array.
variableSynchronizer.Remove(new RemoteVariable(scalarVariable, new uint[] { 10,5 }));
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal