RemoteVariableSynchronizer.Add(variables)

Depending on the overload, adds a variable or a list of variables to the
RemoteVariableSynchronizer
object on which it is invoked.
void public void Add(IUAVariable
variables
); void public void Add(RemoteVariable
variables
); void public void Add(IEnumerable<IUAVariable>
variables
); void public void Add(IEnumerable<RemoteVariable>
variables
);

Argument

variables
(IUAVariable)
The
IUAVariable
C# object to add to the object on which the method is invoked.
variables
(RemoteVariable)
The
RemoteVariable
C# object that identifies a cell of a one-dimensional or multidimensional array to be added to the object on which the method is invoked.
variables
(IEnumerable<IUAVariable>)
The
IUAVariable
list to be added to the object on which the method is invoked.
variables
(IEnumerable<RemoteVariable>)
The
RemoteVariable
list to be added to the object on which the method is invoked.

Examples

In the following example, a variable
speed
is added to the
variableSynchronizer
object.
var speed = LogicObject.Owner.GetVariable("Speed"); var variableSynchronizer = new RemoteVariableSynchronizer(); variableSynchronizer.Add(speed);
In the following example, the index variable
10
is added to the
variableSynchronizer
object within the
arrayVariable
array.
var arrayVariable = LogicObject.Owner.GetVariable("ArrayVariable"); var variableSynchronizer = new RemoteVariableSynchronizer(); variableSynchronizer.Add(new RemoteVariable(arrayVariable, 10));
In the following example, the index variable
10.5
is added to the
variableSynchronizer
object within the
scalarVariable
multidimensional array.
var scalarVariable = LogicObject.Owner.GetVariable("ScalarVariable"); var variableSynchronizer = new RemoteVariableSynchronizer(); variableSynchronizer.Add(new RemoteVariable(scalarVariable, new uint[] { 10,5 }));
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal