InformationModel.MakeAnalogItem(browseName, dataTypeId)

Create a project analog variable derived from
AnalogItemType
, which contains the data type indicated and returns a corresponding
IUAVariable
C# object.
static IUAVariable MakeAnalogItem(QualifiedName
browseName
, NodeId
dataTypeId
);

Arguments

browseName
(QualifiedName)
The
BrowseName
of the new variable.
dataTypeId
(NodeId)
The Data type contained in the new variable.
TIP: A node inside the
DataTypes
class represents the Data type. For example,
OpcUa.DataTypes.Boolean
.

Returns

IUAVariable
A C# object that corresponds to the project variable created.

Example

The following example shows an API that creates an analog variable (
MyAnalogVar
) that contains a float data type:
var myVar = InformationModel.MakeAnalogItem("MyAnalogVar", OpcUa.DataTypes.Float); Owner.Add(myVar);
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal