Import a FactoryTalk Optix Application

To deploy an exported
FactoryTalk Optix Application
, move the file to the target device and run the file.
  1. To import a
    FactoryTalk Optix Application
  2. Move the exported files to the target device.
    For example, attach the USB drive with the exported application to the target device.
  3. Run
    FactoryTalk Optix Application
    on the target system:
    • On
      Windows®
      target devices, in the
      FTOptixApplication
      folder, double-click
      FTOptixRuntime.exe
      .
    • On Linux target devices, in the terminal:
      1. Enter
        cd
        FTOptixApplication
        to navigate to the
        FTOptixApplication
        directory.
      2. Enter
        sudo chmod +x FTOptixRuntime
        to make the runtime executable.
      3. Enter
        sudo chmod +x openssl
        to make the openssl library executable.
      4. Enter
        ./FTOptixRuntime
        to run the application.
    • On
      OptixPanel
      , access the web interface and then select
      Import
      under
      Load application from USB
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal