Users

Users appear as objects in
Project view
. Assign permissions and roles to users to determine the content and interface that the user sees in the application at runtime.
Each project has a default Anonymous user that authenticates the application session. At runtime, the session user is the user who is logged on to the application. The content and UI that appears depends on the visibility set for a group of users or users with a specific role. See Configure security for content at runtime.
TIP: To allow local and domain users to log on, see Authentication. If you set the authentication to Model, Local and Domain, you cannot change the user password or add users. Change the authentication mode to a mode other than Model, Local and Domain.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal