Use translated texts in a string formatter

Create a reference to a translation key to have the key use the related translated text according to the session locale at runtime. A translation key is a reference to a specific translation in the translation dictionary.
  1. In
    Format
    property, type characters present in the key. The keys containing the typed characters appear.
  2. Select a key and then press
    Enter
    .
If the text for the key contains placeholders for the string formatter sources, such as “{0}”), the relative properties appear.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal