Create the System object

The
System
object allows users to view and configure certain system variables, such as the date and time, device, display, and application settings for the
FTOptixApplication
.
Create one
System
object per project.
  • In
    Project view
    , right-click
    Model
    and then select
    New
    All
    System
    System
    .
    System1
    appears in
    Project view
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal