Example interactive session and Presentation Engine

In this example, the start pages in the interactive sessions for
User1
,
User2
, and
User3
are instances of the start page set in the Presentation Engine.
Each start page contains several instances of the same
A
,
B
and
C
objects. The objects are shown or hidden based on the dynamic logics of each user. Text is translated based on the user locale.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal