Idle timeout configuration

Configure a timeout when there is a lack of user activity in the
FactoryTalk Optix
. A timeout can trigger any custom event.
TIP: To configure a timeout, the application must have interactive graphic objects. At runtime, inactivity includes a lack of cursor movements, keyboard actions, and user interactions. You can configure an idle timeout for either a specific page or an entire session.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal