Upgrade a project

You can open a project that was created with a previous version of
FactoryTalk Optix Studio
with later a version by upgrading the project. During the upgrade,
FactoryTalk Optix Studio
creates a backup copy of the original version of the project.
IMPORTANT: After the upgrade, you can no longer open the project with the previous version of
FactoryTalk Optix Studio
. To restore an incorrectly upgraded project, see Restore a project.
  1. Open a project created with a previous version of
    FactoryTalk Optix Studio
    .
    A message appears to request an upgrade of the modules in use.
  2. Select
    Upgrade
    .
    A detailed report of the upgrade process appears.
  3. After reviewing the report, select
    Continue
    to confirm that the project should be upgraded.
FactoryTalk Optix Studio
upgrades and opens the project. In case of any issues, see Troubleshoot upgraded projects.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal