Optix templates
Optix templates provide user-defined default content for projects to contain the same
content as a starting point. You can then create a new project based on the template.
Edit an Optix template by opening the template and modifying the content as desired.
Optix templates have an .optixt extension and are prepended with FTOptix_template_ .
When you create or edit an Optix template, you can select 
Run
to emulate the
template like any other project. You can only deploy a project based on an Optix
template to a runtime device. Provide Feedback