Add a range to a variable

Add minimum and maximum limits to numeric variables. Limits impose certain behaviors when the value is outside of the limits.
  1. In
    Project view
    , select a variable.
  2. In
    Properties
    , right-click the numerical variable name and select
    New
    Range
    .
  3. Under
    EURange
    , complete:
    • Low limit
      . The low limit of the variable value
    • High limit
      . The upper limit of the variable value.
    • Constrain
      . If
      True
      , constrains the values for the variable to the low and high limits.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal